NORD - Moving things together
Getriebebau NORD is one of the world’s leading manufacturers of drive technology
– for mechanical and electronic solutions. The range of products includes geared motors, motors, frequency inverters, motor starters, frequency inverters for decentralised drive control and servo controllers.
NORD CAD 7.0.5
With the latest version of NORD CAD you can now also produce dimensioned and outline drawings as well as 3D models of UNIVERSAL worm gear units SI + SMI according to the catalogue G1035
Energy Saving Calculator
Directly calculate the energy savings for IE2 motors compared with IE1 motors.
National Regulations
National implementation of the IEC standard 60034-30:2008 for the introduction of IE2 motors. The following areas are examined in detail:
Europe, USA, Canada, Australia, New Zealand, Brazil, Mexico, China and Korea
SMART SOLUTIONS
From the very start, NORD DRIVESYSTEMS has aimed to provide complete drive solutions from a single source. We call these SMART SOLUTIONS.
Frequency Inverter - SK 200E
Find out further information about the product innovation from SK 200E on www.sk200e.de
Good cooperation with the crane manufacturer SHB GmbH is greatly appreciated. The procedure is clear. Find out more about the good cooperation between NORD and the customer.
The new SK 9072.1 model is a high-performance 3-stage helical-bevel gear unit with compact dimensions, however with a greater torque capacity and a larger ratio range than is common for the market.
Solarpark Rodenäs
NORD Antriebstechnik auf den Spuren der Sonne - Im Solarpark Rodenäs sind über 700 Universal Schneckengetriebe im Einsatz.