Search | Sales contact
Sales contact
Direct Call: +49(0) 45 32 / 401 - 0
Aluminum replaces stainless steel: NSD tupH from NORD for cost-efficient hygienic drive solutions Bargteheide – NORD DRIVESYSTEMS introduces NSD tupH, a surface treatment that makes aluminum drives as robust as their stainless steel counterparts and which provides a much more efficient anti-corrosion protection than any varnish. Combined with stainless steel standard parts, stainless steel output shafts, and food grade lubricants, NSD tupH drives are the optimal solution for applications with stringent hygiene requirements.
NORD DRIVESYSTEMS Group – global corporate identity to signify expanding international presence The global NORD group currently comprises 35 companies. To document this shared identity, each company from now on will carry the title ‘Member of the NORD DRIVESYSTEMS Group’. The term “drivesystems” is to express the company’s identity as a supplier of comprehensive drive solutions and clearly denote its capacities above and beyond its original line of business manufacturing gears.
NORD at Anuga FoodTec: Drive technology with high hygienic standards At the sixth Anuga FoodTec trade exhibition which will take place March 27-30 in Cologne, Germany, NORD Drivesystems will present itself in Hall 10.1, at Stand B054.
Handling drive-related tasks without external controller For functionally complex and dynamic drive applications, NORD DRIVESYSTEMS announces a new model from its SK 500E line of control cabinet inverters.
Performance bonus for decentralized inverters: SK 200E now up to 22kW NORD DRIVESYSTEMS has extended its SK 200E family of decentralized drive solutions with a new size 4 inverter with a rated power output from 11 to 22 kW.
Grand opening of Australian NORD subsidiary: German drive technology distribution and assembly The inauguration of NORD’s new Australian subsidiary, NORD Drivesystems Pty. Ltd., will take place on 6 October 2011 in the presence of NORD founder G. A. Küchenmeister, Mark Alexander, Managing Director of NORD Drivesystems Australia, and Gernot Zarp, Head of International Sales at NORD.
20 Jahre Fertigungstechnik NORD: Firmenjubiläum und -erweiterung in Gadebusch Am 13. Mai 2011 lud NORD Drivesystems zu einer Jubiläumsveranstaltung ins mecklenburgische Gadebusch ein: Die dort ansässige Unternehmenssparte Fertigungstechnik NORD feierte gleichzeitig ihr 20jähriges Bestehen und die Einweihung des vierten Bauabschnitts, der das Werk auf insgesamt 11.000 m² erweitert hat.
Manual for new motor efficiency requirements: Well-defined flow chart guides users through decision-making process Many drive technology customers are currently in the middle of adapting to the new efficiency requirements for electric motors, while some are only just starting to familiarize themselves with the standards. It is about time to do so: from June 16, 2011, only motors fulfilling IE2 efficiency requirements can be used for certain types of applications within the EU market.
Small, light-weight, versatile: New helical bevel washdown gearboxes At this year's Hannover Messe exhibition, a preview of a new line of performance-optimized two-stage helical bevel gear units will be showcased at NORD Drivesystems' booth. The new units are designed as washdown gearboxes, i.e. cleaning liquids can easily wash off in all installation positions.
SK 500E inverter series now with a 37 kW maximum NORD Drivesystems will shortly add new models to its SK 500E series of cabinet-mounted frequency inverters: The new size 7 inverters cover rated motor outputs between 30 and 37 kW. Models with even larger dimensions are already being planned.
NORD introduces compact high-efficiency motors NORD Drivesystems now provides IE2-compliant three-phase motors delivering outputs as low as 0.55 kW.
Drives for applications with stringent hygiene requirements: New food.nord.com site from NORD DRIVESYSTEMS NORD DRIVESYSTEMS manufactures high-performance, economic drive technology for the food industry.
On-the-spot and in-depth information from myNORD: Online tools at my.nord.com provide access to product and order details At the 2010 Hannover Messe exhibition, NORD Drivesystems launches its myNORD customer portal: this new section of the drive manufacturer’s website, http://my.nord.com, offers on-line tools for registered customers that provide clear and thoroughly detailed information about order status, product selection, local contacts, and latest news. Using easy-to-handle inquiry forms that cover simple to advanced query functions, these intuitive myNORD tools are named DriveExpert, OrderManager, LocatorTool, and Newsletter.
Experience NORD innovations at www.expo-nord.com Online exhibition stand presents new products Bargteheide – With an online virtual exhibition stand, Getriebebau NORD invites you to browse and take a closer look at a comprehensive interactive overview of our complete product range and our latest new product releases. In addition to our wide variety of geared motors, we are proud to include our new large industrial gear units and power electronics for control cabinets and decentral applications.
Production with many facets NORD drive electronics features great depth of production. NORD Electronic DRIVESYSTEMS, a subsidiary of Getriebebau NORD in Bargteheide, has been represented in Aurich since 1984.NORD has invested over 7 million Euro on a new purpose built production facility in Aurich / Schirum which started operation at the end of 2005.
Efficient drive technology For a future-orientated energy budget Continually increasing energy prices make it essential for companies to reduce their operating costs in order to remain competitive. Simply the fact that 2/3 of industrial electricity consumption in production plant is due to drive technology demands a corresponding provision of products and services in order to effectively counteract this problem.
Traffic routes in the production hall Intelligent drive concept for chain conveyor belt system at Audi Doors are produced for the Audi A4 and Audi A5 in a production hall at Audi in Ingolstadt. An extended chain conveyor belt system runs through the almost fully automated production, driven by numerous geared motors, mainly bevelled gear motors due to their high efficiency.
NORD helical gear unit sets new standards An innovation in drive technology Getriebebau NORD is one of the leaders in the field of drive technology. This is demonstrated once again by the introduction of NORDBLOC.1 inline helical gear unit, which the company from Bargteheide is really excited about.
Ethernet connection for NORD frequency inverters NORD offers new solutions for the growing number of drive system users who are choosing Ethernet-based fieldbus connections for automation tasks.
Optimized for high loads: Powerful helical bevel geared motors in an FEM-calculated housing The UNICASE housings of NORD's new three-stage type SK 9096.1 helical bevel geared motors have been optimized through FEM calculations, ensuring cost-efficient production and high load capacity.
Growing family of SK 5xxE frequency inverters: Extended model range now consists of six sizes NORD has extended its SK 5xxE line of frequency inverters by new size 5 and 6 models. Thereby, new performance ranges have been added:
Energy-saving inverters with magnetization adjustment option More efficient operation of AS motors with optimized motor current SK 5xxE type frequency inverters can save resources by automatically reducing the magnetization of an asynchronous motor when the motor is operated under partial load.
Giants in a UNICASE housing: New industrial gear units with max. torques up to 200,000 Nm NORD has extended its range of industrial gear units, adding new models with maximum torques of 60,000 Nm, 90,000 Nm, 135,000 Nm and 200,000 Nm. NORD is the only supplier worldwide to construct even 90,000 Nm and beyond models according to the proven UNICASE concept.
Expertise for energy-efficient drives: Three ways to ensure optimal savings Success in developing highly efficient drives depends on seizing energy saving potentials in gearboxes, motors and power electronics alike.
Cost-efficient drive solutions for hazardous areas with Ex e motors certified for inverter operation Gas explosion-protected drives in “increased safety” (Ex e) from NORD are blanket approved for operation with a frequency inverter. Users can thus tap high savings potentials:
Introducing the decentral SK 200E: Integrated drive units for price-sensitive applications NORD extends the flexible NORDAC DA series of decentral drive components, adding the new type SK 200E frequency inverters which were first presented at this year's Hannover Messe trade show.
Powerful positioning control with NORD frequency inverters Bargteheide – Applications which require relative or absolute position control (e.g. rotating platforms, linear movement axes or synchronised positioning) can be quickly and economically implemented with NORD standard asynchronous motors and frequency inverters. The drive specialist NORD supplies several series of inverters with integrated POSICON intelligent positioning, which in many cases can even replace servo solutions. The position control provides a wide range of functions, is easy to operate and can easily be parameterised without any knowledge of complex programming languages.
Safety first: NORD frequency inverters feature Many machines and plants, e.g. machine tools such as milling machines, need to fulfill strict operator safety standards: when a safety circuit is activated, operators must be safe from rotating machine parts.
Fieldbus connection options: NORD frequency inverters support Ethernet NORD Drivesystems, a full-line supplier for drive technology, offers the NORDAC SK 500E and SK 700E inverter series which cover the complete spectrum of standard, enclosure-mounted intelligent frequency inverters.
Robust gearboxes and geared motors Drive systems from NORD provide high precision and a long lifespan owing in particular to the geared motors' UNICASE design, which was developed by the company in 1981.
Full-line service provider for drive technology NORD Drivesystems, founded in 1965 in Bargteheide near Hamburg, Germany, manufactures and distributes mechanical and electronic drive technology.
Easy position control with NORD frequency inverters NORD's standard asynchronous motors and frequency inverters allow for the quick and cost-efficient implementation of applications requiring relative or absolute position control (e.g. rotary tables, linear travel axes or synchronous speed control).
Increased safety (Ex e) protection for inverter-controlled motors enables more costefficient, lighter ATEX drive solutions NORD has expanded its ATEX product lineup to include a new area of application: gas explosion-protected drives featuring “increased safety” (Ex e) which are generally approved for speed-controlled operation with a frequency inverter.
Eco-friendly and cost-saving: Energy efficient drives from NORD Already since 1995, NORD DRIVESYSTEMS has been providing system solutions consisting of motors, gears and intelligent electronic controllers which optimize energy use throughout the power train.
SK 530E: Standard frequency inverter with high-performance features NORD presents the new SK 530E type frequency inverter, which offers an excellent price-performance ratio and the functionality of a high performance inverter, thereby extending the proven SK 5xxE series.
NORDAC DA: system components for decentral drive solutions Decentral drive technology simplifies the layout of plants and minimizes the required space and expenses.
NORDAC SK 500E/520E/530E: Compact frequency inverters for a wide range of applications The compact frequency inverters NORDAC SK 500E/520E/530E come with a wide range of basic features and can be easily adapted to specific applications.
Für anspruchsvolle Applikationen: Servoregler NORDAC SK 1000E Der NORDAC SK 1000E verfügt über vollständig digitale DSP-Technik und ein feldorientiertes Regelkonzept, das bei Abtastzeiten von lediglich 50 µs auch höchste Dynamikanforderungen erfüllt.
Universally applicable: NORDAC SK 700E NORD’s SK 700E frequency inverters, which belong to the tried-and-tested NORDAC line, are specified for a mid-to-upper level power range between 1,5 and 160 kW.
Stronger, lighter, more compact: New NORDBLOC type geared motors NORD Gear has enhanced its compact line of UNICASE geared motors through design improvements.