Recherche par mot clé | Contact vente
Contact vente
Téléphone: 888-314-6673
Vous trouverez ci-dessous des articles de presse et des photos concernant notre société et nos produits, ainsi que des informations sur nos prochains salons et foires.
New approaches for better energy economy Bargteheide – Savings are a big issue in all industry branches, today more than ever, which leads many users to try and reduce the power consumption of drive systems. However, such considerations should not merely focus on optimizing the consumption of individual electric motors, but should instead encompass drive systems solutions as a whole. Providing user-specific, customized energy saving concepts, drive expert NORD ensures maximum cost efficiency and eco-friendliness. NORD employs a wide range of technologies to this end, including regenerative braking, automatic magnetization adjustment, copper rotors, 87 Hz operation, and intermediate circuit coupling.
NORD helical gear unit sets new standards An innovation in drive technology Getriebebau NORD is one of the leaders in the field of drive technology. This is demonstrated once again by the introduction of NORDBLOC.1 inline helical gear unit, which the company from Bargteheide is really excited about.
Production with many facets NORD drive electronics features great depth of production. NORD Electronic DRIVESYSTEMS, a subsidiary of Getriebebau NORD in Bargteheide, has been represented in Aurich since 1984.NORD has invested over 7 million Euro on a new purpose built production facility in Aurich / Schirum which started operation at the end of 2005.
Efficient drive technology For a future-orientated energy budget Continually increasing energy prices make it essential for companies to reduce their operating costs in order to remain competitive. Simply the fact that 2/3 of industrial electricity consumption in production plant is due to drive technology demands a corresponding provision of products and services in order to effectively counteract this problem.
Traffic routes in the production hall Intelligent drive concept for chain conveyor belt system at Audi Doors are produced for the Audi A4 and Audi A5 in a production hall at Audi in Ingolstadt. An extended chain conveyor belt system runs through the almost fully automated production, driven by numerous geared motors, mainly bevelled gear motors due to their high efficiency.
Introducing the decentral SK 200E: Integrated drive units for price-sensitive applications NORD extends the flexible NORDAC DA series of decentral drive components, adding the new type SK 200E frequency inverters which were first presented at this year's Hannover Messe trade show.
Variateurs de fréquence à économies d’énergie avec l’option d’ajustement de la magnétisation Un fonctionnement plus efficace des moteurs asynchrones avec l’optimisation de l’intensité moteur Les variateurs de fréquence de type SK 5xxE peuvent économiser de l’énergie en réduisant automatiquement la magnétisation d’un moteur asynchrone triphasé lorsque le moteur fonctionne sous charge réduite. Le courant moteur est en conséquence ajusté selon les besoins et les pertes par effet joules sont minimisées.
Expertise for energy-efficient drives: Three ways to ensure optimal savings Success in developing highly efficient drives depends on seizing energy saving potentials in gearboxes, motors and power electronics alike. NORD has been following this integrated approach since the mid-1990s in all efforts to supply drive units with optimized overall efficiency.
L’optimisation pour les charges élevées : Motoréducteurs puissants à couple conique dans un carter garanti par les calculs FEA Le carter MONOBLOC du nouveau motoréducteur à couple conique à trois trains SK 9096.1 de NORD a été optimisé par le calcul des éléments finis (FEA), garantissant ainsi une production optimisée et une capacité de charge élevée.
La famille des variateurs de fréquence SK 500E s’agrandit : un large choix de modèles est disponible à présent en six tailles différentes La gamme des variateurs de fréquence SK 500E de NORD Réducteurs a été étendue avec les tailles 5 et 6. Ainsi la déclinaison des classes de puissance s’est étoffée : en plus des variateurs de fréquence de puissance de 0,25 à 7,5 kW, les utilisateurs disposent dorénavant d’un choix de variateurs de fréquence allant jusqu’à une puissance de 22 kW.
Connexion Ethernet pour les variateurs de fréquence NORD NORD propose de nouvelles solutions au nombre croissant d’utilisateurs ayant choisi une connexion par bus de terrain basée sur l’Ethernet industriel pour les tâches d’automatisation.
Cost-efficient drive solutions for hazardous areas with Ex e motors certified for inverter operation Gas explosion-protected drives in “increased safety” (Ex e) from NORD are blanket approved for operation with a frequency inverter. Users can thus tap high savings potentials:
Des capacités gigantesques dans un carter MONOBLOC : Nouveaux réducteurs industriels avec des couples jusqu’à 200 000 Nm NORD a étendu sa gamme de réducteurs industriels en ajoutant de nouveaux modèles dont le couple maximal atteint 60 000 Nm, 90 000 Nm, 135 000 Nm et 200 000 Nm. À l’échelle mondiale, NORD est le seul fournisseur qui fabrique des modèles de 90 000 Nm et plus, suivant le concept éprouvé du carter MONOBLOC.
La sécurité avant tout: «arrêt sécurisé» intégré sur les convertisseurs de fréquences NORD Lors de l'exploitation de nombreuses installations, p. ex. de machines-outils comme des fraiseuses, la sécurité des personnes est essentielle : une fois un dispositif de sécurité activé, aucune partie mobile de l'installation ne doit mettre en danger l'opérateur.
Choix pour la connexion des bus: les convertisseurs de fréquence NORD prennent en charge Ethernet En tant que fournisseur global de solutions d'entraînement, Getriebebau NORD propose à ses clients toute la gamme des convertisseurs de fréquences intelligents classiques, installés de façon centralisée, avec les séries SK 5xxE et SK 700E.
Fournisseur global de solutions d'entraînement Getriebebau NORD, société fondée en 1965 à Bargteheide, près de Hambourg, produit et vend des solutions d'entraînement mécaniques et électroniques. L'entreprise – aujourd'hui l'un des leaders de son secteur – offre une large gamme de produits qui, outre des réducteurs et des moteurs électriques, comprend également des systèmes à électronique de puissance de régulation et de commande.
interactive tools a réalisé le nouvel accès à NORD sur Internet www.nord.com donne de nouvelles impulsions aux fabricants de machines dans le domaine des entraînements Le nouveau site Web de Getriebebau NORD suscite l'enthousiasme des ingénieurs: des grues géantes dans des installations portuaires ou des structures de toit mobile dans des stades modernes, le deuxième plus grand fournisseur mondial de solutions d'entraînement, de moto-réducteurs et d'électronique de puissance n'est pas seulement présents dans de tels projets gigantesques.
Sécurité renforcée (Ex e) pour moteurs à convertisseur de fréquences: nouveaux entraînements ATEX plus légers et plus économiques Getriebebau NORD a étendu le domaine d'application de sa gamme ATEX : entraînements protégés contre les risques d'explosion avec une « sécurité renforcée » (Ex e), généralement autorisés à fonctionner avec un convertisseur de fréquences. Les moto-réducteurs sont jusqu'à 25 % plus légers et jusqu'à 40 % moins chers que les entraînements avec « enveloppe antidéflagrante »(Ex de).
Un envoronnement meilleur et des réductions de coûts: Entraînements à haut rendement de NORD Réducteurs Depuis 1995, NORD Réducteurs fournit des solutions d’entraînement, moteurs, réducteurs et variateurs de fréquence dont les rendements ont été optimisés. Par rapport aux entraînements conventionnels, les coûts de fonctionnement de ces matériels peuvent diminués jusqu’à 40%.
Outil universel : SK 700E Les convertisseurs SK 700E de la gamme NORDAC éprouvée sont conçus pour les plages de puissance moyennes et supérieures, entre 1,5 kW et 160 kW.
SK 500E/520E/530E: Les variateurs de fréquence compacts aux larges champs d’application Les variateurs de fréquence compacts SK 500E/520E/530E possèdent des caractéristiques de base étendues et peuvent être adaptés aisément aux applications spécifiques.
NORDAC DA : Composants système pour solutions d’entraînement décentralisées La technologie décentralisée des entraînements simplifie la structure des installations, diminue l’encombrement et réduit les coûts. Le concept de décentralisation NORDAC-DA offre à NORD toute la souplesse permettant d’extraire le système de commande électronique de l’armoire électrique pour le placer directement au niveau de l’entraînement.
Plus robustes, plus légers, toujours plus compacts: La nouvelle conception des motoréducteurs à carter monobloc NORDBLOC Grâce à une construction novatrice mais toujours sur la base du concept Monobloc, le groupe NORD a développé une nouvelle génération de réducteurs à engrenages cylindriques NORDBLOC, en lui apportant de nombreuses améliorations, qui font toutes l’objet de brevets.
Réglage d'assiette facile avec les convertisseurs de fréquence NORD Les applications nécessitant un réglage d'assiette relatif ou absolu (p. ex. tables rotatives, axes de positionnement linéaires ou régulation synchrone) peuvent être mises en œuvre rapidement et de façon économique à l'aide de moteurs asynchrones standard et de convertisseurs de fréquence Getriebebau NORD.